This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS7843 - Problem

Other Parts Discussed in Thread: ADS7843

Hello:

           I get the following problem with the tocuh controller ADS7843, when use capacitores for noise filter on X+,Y+,X-,Y- inputs. If the capacitores are present we can not move the cursor properly. Because mismatch exist between the pen and the cursor on the touch panel.

The funcion used for calibrate is tc_calibrate and the funcion used for test is ts_test  my system is linux 2.6.27.5 and ts.lib 1.0.  The circuit is the same that appears in the application note "Touch Screen Controller Tips"  http://focus.ti.com/docs/prod/folders/print/ads7843.html 

If i take the capacitores and the TVS all work fine, but i need protect that input.

best regards