art Number: ADS8555
Hello team
The following question came from a customer to Japan CSC.
I set Control Register in 0x0043 03FF.
C22 A-NAP:1 = Auto-NAP feature enabled
C17 READ_EN:1 = Control register contents output on SDO_x with next access
C16 C23:0_EN:1 = Entire control register update enabled (serial mode only)
Bit except the above is a default value.
Value becomes 0x7FFE 7FFE when I read a value of CR in the following procedures.
Procedures:
①With FS as Low, I send SCLK for 96bit.
②value of SDO becomes value unlike 0x7FFE 7FFE.
(I attach a wave pattern of SCLK,SDI,SDO at that time.)
Please tell me the right procedure to read a value of CR.
For example, with CONVST_A as High, BUSY becomes High and becomes Low.
At that time, is a value of CR readable from SDO_A if I input SCLK 32?
Best regards,
Keishi,Nishijima
Japan CSC