Other Parts Discussed in Thread: ADS1282
I have a few questions about the ADS1281 Analog to digital converter:
- Table 5 specifically says the rates provided are for a 4.096 MHz clock. Table 6 doesn't explicitly state that. Should we assume that the rates in Table 6 are for a 4.096 MHz clock and scale them accordingly when we use a slower clock, or are they absolute?
- Is there any kind of pipe-lining in the output stream? We have a mux before the input to the ADC and are having some timing issues. We understand that the FIR output requires 63 cycles to settle after we swtich the mux. (We are running in Continuous-Sync Mode.) Does that mean we need to wait for 63 DRDY pulses or is that delay already included? When is the best time to swtich the mux?
- How do we set the device for 24-bit output data?
Thanks,
--Dean Palmer