Part Number: AFE5851
Hi,
I have an image application that needs 32 analog inputs. I designed it with two AFE5851 chips. The analog input is driven by an amplifier output with 50 OHM serial resistor directly. The amplifier output is 1.1VDC plus 0 ~ 1V AC signal.
My question is: If all the 32 channels are with 1.5VDC input, could the AFE5851 provide the correct digital readings?
Best,
Xiuyan