This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC12D1800: Out of Range Behavior in Two's Compliment mode.

Part Number: ADC12D1800


Section 6.1.1.4 states that when an Out of Range condition is detected the data output will be all '1's or all '0's depending if it is over range or under range.  This is consistent with the default output format of offset binary.  Does the output during Out of Range conditions change to '0111_1111_1111' and '1000_0000_0000' when in two's compliment mode?