Hi,
I'd like to keep the DCLK running all the time even during ADC calibration. According to datasheet pg 8/53 this is possible but Resistor Trim portion of calibration should be disabled after the very first power-on calibration cycle.
"If a system requires DCLK to run continuously during a calibration cycle, the termination resistor trim portion of the cycle can be disabled by setting the Resistor Trim Disable (RTD) bit to logic high in the Extended Configuration Register. This disables all subsequent termination resistor trims after the initial trim which occurs during power-on calibration. This output is not recommended as a system clock unless the resistor trim is disabled."
I am using the ADC07D1520 in Extended Control Mode with non of the parallel control pins connected.
** what are the side effects of disabling Resistor Trim calibration portion?
** Will the rest of calibration be fine??
** DCLK+/- will be running continuously, as datasheet says??
Please advise.
Thanks,
-Reza