Part Number: THS12082
Hi
I'd like to know the max. single end input range of THS12082.
As per datasheet, the recommended setting would be
VREFP=3.5V and VREFM=1.5V and you get the input range of VREFP-VREFM=2V.
In single end config, can I tie VREFM to AGND and VREFP to AVDD(5V) and hope to get max. single end input rang of 5V?
Would it be still working?
Looking forward to an anwser. Thanks.