Hello guys,
So I am using ADS1120 to measure the thermocouple temperature. As I was referring to the manual I came across the section 9.2.1.3 Application curves which speaks about a system offset calibration performed to translate Vtc to 0V. Can anyone explain what kind of offset calibration was it? As I am trying to measure the K type thermocouple temperature, I get some absurd values after I perform the cold junction compensation as mentioned in the manual.
My ambient temp is 22.5 deg C and for testing purposes I am measuring an object with 30 deg C temperature (this is the hot junction).
Can anybody help me with this?
Thanks,
Regards,
Kartik