Part Number: AMC1210MB-EVM
Other Parts Discussed in Thread: ADS1203, AMC1203EVM,
I try to evaluate ADS1203 ADC in combination with an AMC1210MB-EVM i bought recently. I have built a custom EVM with similar wiring and pinnning as AMC1203-EVM. I have chosen Mode 0, so internal clock and synchronous data output with Pins M1 and M0 connected to GND.I have observed on scope correct 5V Bitstream on Pin9/8 (jumpersetting) and 10MHz clock signal on Pin 7/6 of the DSUB9. I use the 5V supply from the AMC1210MB-EVM, as the ADS1203 needs 5V and not 3.3V as the.AMC1203EVM.
I have installed the software on an old WinXP-System and it seems to be able to connect with the EVM. Unfortunately it responds "Firmware encountered an unexpected failure, please try again" whenever i try to aquire data. Variation of settings would not help so far.
I hope, you can provide a hint , what is going wrong.
best regards, Matthias