Part Number: DAC8734
*DAC 8734 READ Questions*
1.Voltage on DAC 8734 READ
->The voltage used for DAC control is (DVDD (+ 5v) / IOVDD (+ 3.3v) / AVDD1,2 (VDD + 15v) / AVSS1,2 (-15v)).Of the four voltages, only DVDD + 5v / IOVDD (+ 3.3v) is supplied to the DAC.
In case of DAC READ, we ask if AVDD1,2 (VDD + 15v) / AVSS1,2 (-15v) should be applied to DAC.
2.Is the DSDO signal to be 1 when writing? If it is set to '1', should it be controlled to '0' when it is read and read?
3.Resister map for DAC when wirte
(x"00" x"0080") DSDO : '1'
(x"04" x"4000")
Resister map to DAC when read
(x"84" x"0000")
Write to dac on 24bit 1cycle dac.
cs: high -> low -> high
clk: low -> 24clk -> low
data low -> 24data ->low
If read, should CS be applied to dac for 2 cycles? E.g
cs: high -> low -> high -> low-> high
clk: low -> 24clk -> low -> 24 clk->low
data low -> 24data ->low-> 24data -> low
thank you