Part Number: ADS1278
I would like to interface the ADS1278 with the AM335x. According to the section 22.2 the AM335x has two instantiations of the McASP subsystem: McASP0 and McASP1. Each of one with 4 serializers AXR[0:3]. The ADS1278 however has 8 channels. I want to use the max data rate (144kSPS), if possible, trying to avoid TDM mode, using instead Frame-Sync discrete mode. My question is, if using an external oscillator to feed both McASP0 and McASP1, can I "merge" them to use the 8 channels in parallel, i.e., 4 channels for McASP0 and 4 channels for McASP1 ? Or the only way is using TDM mode?
Thank you in advance.