Part Number: ADS1115
Hi
I'm developing my own device which uses ADS1115. I'm using connection as in the picture below. I configure ADS1115 as follows:
adcInitConf.compQue = COMP_QUE_ONE;
adcInitConf.compLat = COMP_LAT_ENABLE;
adcInitConf.compPol = COMP_POL_HIGH;
adcInitConf.compMode = COMP_MODE_WITH_HYSTERESIS;
adcInitConf.dr = DR_128_SPS;
adcInitConf.mode = MODE_SINGLE_SHOT;
adcInitConf.pga = PGA_6_1;
adcInitConf.mux = MUX_0_G;
adcInitConf.osWrite = OS_WRITE_BEGIN;
I'm waiting for 'alert/rdy' pin is high and read value from ADC. It works is well but if ADS1115 input is not connected or connected to ground ADC don't set 'alert/rdy' pin. In this case, I expect to get a zero value.
Any ideas? Is any additional information required?
Thanks very much,