Part Number: ADS1298
Hi,
I have a ADS1298 in a simple system with 1 channel enabled, gain = 12, bipolar power supply (+2.5, -2.5), 1Ksps ADC, RLD output driven from CH1+/-.
My device is battery powered and not connected to any mains powered devices and is very similar in design to the ADS1298ECGFE-PDK
I am using the device in a surface EMG application. On a limb I have a pair of electrodes spaced about 50mm apart over a muscle and at the end of the limb I have the RLD electrode. Electrodes are connected to my hardware via shielded cables with SMA connectors.
The data I've collected from the ADS1298 shows about 250uV of 50Hz noise, and this is about 25% of my signal, which is really bad. The noise is not present when I short the electrodes together.
I've had a look at sbaa188.pdf and I notice an anomaly between the ADS1928EVM's input filters (of 47pF capacitors) and the sbaa188.pdf's values of 47nF.
I'm interested to know what the best route of determining how the 50/60Hz noise is getting into the system and what is the best way of dealing with it.?
If I want to measure the CMRR could I simply set the gain to 1, join CH1 +/- together at the electrodes and inject a 10Hz, 1Vp-p signal?.
If I measure the Input and capture the output signal from the ADC, would this be accurate enough for a CMRR measurement? and therefore would the CMRR measurement give me a better indication if the 50/60Hz noise is getting into my system based on some poor CMRR value?
Thanks
Stomp!.