I want to use the ADC12DJ2700EVM with ZC706.
Unfortunatley, I had a mistake, and I did not find connector difference of two boards.
The ADC12DJ2700EVM only has a connector of FMC+, but the ZC706 has a connector of FMC HPC and FMC LPC.
So, I have two questions.
1. Can I connect two board focibly througth removal of the outer of the ZC706 connector?
I checked pin out of the ADC12DJ2700EVM, and I found that the focible connection is possible if I only use 8 lanes for the JESD204B. Right?
2. If two board can be connected (it means I use only 8 lanes for the JESD204B), can I use them at sampling rate of 5.4 GHz and transfer the sampled data to ZC706 board?