Other Parts Discussed in Thread: ADS1262
Hello,
We are working on ADS1263 adc which has maximum sampling rate of 38400 SPS as per datasheet.
So, technically we should get number of sample per cycle=Sampling rate/ Input frequency.
E.g. For 10 Hz input sinusoidal signal, sampling rate after setting 38400 SPS, we should get 3840 samples.
But in this condition we are getting 510 samples.
After checking datasheet again we found that conversion latency of Sinc5 filter for 38400 sampling rate (page number 63 Table 17. ADC1 conversion latency).
We also found that new data is available as per this latency only i.e. after
0.207 ms for 38400 SPS.
We would appreciate if you clarify on this, if sampling rate is mentioned 38400, we should get output samples according to it.
What role does the Sinc5 latency plays in getting digitized data?