Hello E2E Forum,
I am aware that this IC should not be used for medical applications. However, I was wondering if there were any protective measures built-in to the device other than for ESD.
Thank you,
Danny
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello E2E Forum,
I am aware that this IC should not be used for medical applications. However, I was wondering if there were any protective measures built-in to the device other than for ESD.
Thank you,
Danny
Hi Danny,
Thank you for your post and welcome to our forum!
The ADS1299 ABSOLUTELY can be used in medical applications. The catch is that medical device standards apply to the whole system, not just one component. The ADS1299 is a great fit for low-noise biopotential applications, such as EEG or even fetal ECG, but additional circuitry is required to satisfy any and all regulatory standards for safety and performance. Other than ESD, the ADS1299 does not include any other protective measures.
Best Regards,