Other Parts Discussed in Thread: ADS1230, ADS1232, ADS1231, ADS1220, ADS1235, ADS124S06
Hi Everyone,
I am planning to use the AD1246 with a load cell at 3.3V operation.
1. Can is still use the the 2.048V reference or is it better to use an external reference?
2. Is there an effect on the effective number of bits (ENOB)? Based on my computation so far, i loose dynamic range by using a 3.3V instead of 5V but is the ENOB still the same? Based on the datasheet, the ENOB is only affected by the reference voltage. However, according to this application note SBAA184, i need more bits due to the difference in the full scale range and the dynamic range of the loadcell input.
Thanks,