This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8350: VOL with external pull-up

Genius 17525 points
Part Number: ADS8350


Hello,

 

I have a question for ADS8350 VOL specification.

 

Now I have to add external pull-up on SDO-x line for some reason.

Then I want to understand acceptable pull-up resister value range.

 

The datasheet defines VOL MAX as 0.2 DVDD where the condition is I_OH=500uA sink.

Assumed DVDD=3.3V, it means that over 6.6Kohm is acceptable for less than 0.2 DVDD VOL.

 

On the other hand, Input current of Absolute max is defined as +-10mA in the datasheet.

It means 330ohm for DVDD=3.3V.

 

From these two definition, for DVDD=3.3V case,

1. Over 6.6Kohm                     : TI guarantees that VOL=0.2DVDD.

2. From 330ohm to 6.6Kohm  :  The user can use it, the device will not have any reliability issue. But not sure for VOL value, it's user's risk. 

3.  Less than 330 ohm            :  Over abs max, it could be broken and have a reliability issue.

Is this my understanding correct?

Regards,

Oba