This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC38RF82: External Reference

Genius 12865 points

Part Number: DAC38RF82

Hello Team,

the DAC38RF82 has a built-in reference voltage for the DAC core of 0.9V. The reference voltage can be measured on the pin EXTIO.

According to the datasheet, this pin is I/O. Is it possible to use an external 0.9V as reference voltage? What are the current drive requirements for an external reference to override the internal reference?

Thanks and Best Regards,

Hans