This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1292R: Plz, help me.

Other Parts Discussed in Thread: ADS1292R, ADS1292

art Number: ADS1292R

I'm not used to Eng.

I can read test signal well. 

*Sampling rate 250Hz

y-axis is mV, x-axis is sample number.

But I can't read correct signal from electrodes that were connected with CH1. and the signal was 3Hz-50mVpp-Sine wave from function generator.

*Sampling rate 500Hz.

y-axis is mV, x-axis is sample number.

It is similar 3Hz(three periodic wave in 500 samples, 1 sec) but with only positive polarity. and also the amplitude is not correct.

So I changed polarity of input cable. then,

 ...

I want to read whole sine wave. why these error occurs? my schematic is

VREF was well measured at 2.42V

and register set 

write_reg(0x01, 0b10000010);
write_reg(0x02, 0b10100000);
write_reg(0x03, 0b00010000);
write_reg(0x04, 0b00000000);
write_reg(0x05, 0b10000000);
write_reg(0x06, 0b00000000);
write_reg(0x07, 0b00000000);
write_reg(0x08, 0b00000000);
write_reg(0x09, 0b00000000);
write_reg(0x0A, 0b00000011);
write_reg(0x0B, 0b00000000);

plz, help me.