This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE4490: the maximum switching speed for LED driver in AFE4490

Part Number: AFE4490

Hi 

How about the maximum switching speed for LED driver in AFE4490? Can it support 10Khz switching speed?

If only one LED is needed, can it work with below configuration to double switch speed?

Thanks.


  • Hi Oliver,

    The frequency of the LED in AFE4490 is governed by PRF (i.e. once in every PRP cycle).
    For the scheme as shown above, the LED will be switched twice in a PRP cycle and if you set the PRF = 5KHz the switching frequency of the LED will be 10KHz.

    Regards,
    Prabin