This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC5652AEVM: Configuration and setup for Zedboard and DAC5672evm

Part Number: DAC5652AEVM

Hi,

I have the following configuration:

1) Zed board connected as data source; output = 1MHz 14-bit sine output.

2) TCXO generating 40MHz LVCMOS output as clock reference.

3) DAC5672EVM.

Not getting the sinusoidal output from the DAC5672EVM.

Connection made as per user manual for DAC5672/62/52 14- and 12-Bit Dual Channel DAC EVM (Rev. B).

Please help in debugging!