Other Parts Discussed in Thread: LMK04828, DAC38RF80
Hello,
When configuring the DAC38RF80EVM (such as interpolation rate, clock frequency, etc.), do the settings remain on the board when power is cycled or will it have to be reprogrammed each time? There is no easy way to tell with the GUI as you can't read and upload current configuration parameters into the program (a possible software improvement for a future revision)
And to verify, the board's configuration settings can be programmed through the FMC connector using the JESD204 standard correct?
Thanks,
Jared