This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS7817: Bandwidth data

Part Number: ADS7817
Other Parts Discussed in Thread: ADS8350

Hello,

 

I would like to know the bandwidth information of ADS7817, especially -3dB case.

Like ADS8350 defines Full-power bandwidth as 25MHz at -3dB and 5MHz at -0.1dB in the datasheet.

Is this kind of data for ADS7817 available?

 

Regards,

Oba

  • Oba-san,


    I've checked and there isn't an data on full-power bandwidth for the ADS7817. The ADS7817 was introduced in 2001, and I could not find any old characterization data for this device, other than what is shown in the datasheet.


    Joseph Wu