Part Number: ADC128S102
Hello,
we are using ADC128D102 for fast Multiplexed Data Acquisition system and we want to convert analog data coming from 64 x 64 matrix, samples that are coming from my multiplexed circuit is 1 mega samples per second on all 8 channels of ADC and i want to read this 1 Mega samples per second data using all 8 channels of ADC in 1 second and as per datasheet of this ADC128 it can sample 1 mega samples per second , but i am facing problem while reading data because i am not able to read 1 mega sample per second using all 8 channels of ADC.
please give me some suggestion on this that how can i able to read 1 mega samples of data per second coming from my system on all 8 channels of adc.
I have done some testing experiment on ADC128S102, so i was testing this ADC with raspberry pi and i took readings for 1MSPS samples on a single channel which took almost 17 Sec , but as per datasheet ADC128 is able to sample 1MSPS samples per sec i.e. 1MSPS is a sampling speed of ADC128 with 16 Mhz of clock frequency,
So my questions are 1) How to achieve 1Msps of speed on single channel of ADC128 ? ,because as per my testing i got only 97646 samples per second which is less than mentioned in datasheet
2) How much speed we can achieve per channel while using all 8 channels of ADC?
3) How to set Clock frequency of this ADC to its Maximum Allowed Frequency which is 16MHZ in this case to achieve 1msps ?
4) How to increase and decrease sampling rate of this ADC, if i want to decrease sampling rate to 500ksps what should i do?