This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC128S102QML-SP: maximum output current

Part Number: ADC128S102QML-SP

What is the specified maximum output current for ADC128S102QML-SP for source and sink?  The data sheet only lists Voh and Vol test conditions of 200uA and 200uA to 1mA respectively.  The data sheet implies that is can source 200uA maximum.  This would imply that it may not operate within specifications with a 3.3V supply and a 10k ohm resistor to ground.

Thank you for your reply!