Other Parts Discussed in Thread: ADS1278
Hello,
My understanding is that the SYNC input is only used to synchronize multiple devices with each other or to synchronize the device(s) to an external event. Can someone please provide any other situations (if any) that require the SYNC input to be used. For example, if the clock inputs are interrupted is asserting SYNC ever necessary with a single device? Also, the datasheet says: "For consistent performance, re-assert SYNC after device power-on when data first appear." Does this only refer to synchronizing multiple devices being used together after power-on?
We are using a single ADS1278 in our design which will run continuously. Is there any reason whatsoever that we wouldn't want to simply tie the SYNC pin to IOVDD?
Thanks,
Kal