This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TSW1400EVM: TSW1400EVM

Part Number: TSW1400EVM
Other Parts Discussed in Thread: ADS5294, ADS5294EVM

Hi,

we are interfacing ADS5294 Evaluation board with TSW1400EVM 

we are tried generating ramp in ADS5294 GUI and Captured Time domain Data in HSDC pro software 

we are getting following ERROR

"Frame Clock Error in read DDR to file".

Can anyone help us solve the above Issue

Thanks

Prateek

  • Prateek,

    I have forwarded your question to a device expert. They should be with you shortly.

    Thanks

    Yusuf
  • Hi Prateek,

    Thanks for using ADS5294EVM + TSW1400EVM.

    (First thanks to Yusuf for forwarding this E2E.)

    Seems like there are some board connection issue happened.

    Please take a look and check the following examples.

    And see if your EVM connections are the same

    Hope this can make your board running correctly.

    Thank you!

    1) Please make sure all the jumpers on your ADS5294EVM are connected as the follows.

    (Note: right now the jumper connections are using the on-board Clock. Therefore no external clock is needed right now.)

    2) Please check all the wire connections between ADS5294EVM + TSW1400EVM

    are following below (including power supplies, USB to your PC, input signal connection):

    (Note: right now the external input clock is not needed for this Jumper connection example)

    Thank you

    and best regards,

    Chen