These questions have been posted by one of my customers a while ago. He never received an answer.
Here they are again:
The following questions are to help me to understand how behave the TSC2006 when it’s throughput (batch delay) is faster than the rate at which the processor read the X/Y coordinates. The Window CE driver that is available on the TI web site use the TSC2006 in that mode.
- When the TSC2006 finish processing a new X/Y coordinate but the processor has not read the previous coordinate is the new coordinate overwrite the previous one?
- When the processor read the previous X/Y coordinate after the TSC2006 has finish processing the new Y coordinate but not the new X coordinate is it guarantee the X and Y position the processor get come from the same conversion cycle?
- When the processor read an X/Y coordinate at the exact same time the TSC2006 is updating its X and Y registers is the data the processor will get be valid? Is it guarantee the X and Y position the processor get come from the same conversion cycle? Is the content from X or Y register can be corrupted?
The following questions are regarding the test conditions for the VOH and for the VOL of the TSC2006.
- In the data sheet, the test conditions say IOH and IOL are 2 TTL loads but I don't know what is a TLL load. What are the IOH and the IOL current for one TTL load? Is the magnitude of IOH and IOL are the same?
- There is no IBIS model for the TSC2006 but there is one for the TSC2008. Is the IBIS model for the SDO and PINTDAV outputs of the TSC2008 can be use for the TSC2006.
Teodor