This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/ADS7953: ADS7953 range from 2.5 to 5V issue

Part Number: ADS7953

Tool/software: WEBENCH® Design Tools

Hi,

I am trying to program ADS7953 to auto1 mode with range 2 i.e. 0 to 5 V with following sequence

>> wr 0x4200

>> wr 0x8000 

>> wr 0xFFFF

>> wr 0x2C40

>> wr 0x000 all

But when i vary my potentiometer connected to channel 4 at 2.5V itself the ADC converted value gets set to 4095 whereas it should get set to 2046 i.e half of the 5V count.

I am able to change from 2.5 to 5 V in manual mode by writting 0x1840 in mode register but not able to change in auto mode 1. 

How can i verify that my device has switched to auto mode1?

is the sequence that i am writiing to change to auto mode1 and range 5v right?

Thank you

Regards,

Chandrakant Pal