Part Number: ADS1217
Everything seems to be working ok,
but I dont know why the DRDYn pin is always driving this signal even after power up!!!
Below pin status: (I am not issuing any commands to ADC)
CSn = high
SCLK = low
CLK = 8MHZ
DIN = low
DSYNC = high
DOUT = low
POL = low
RESETn = High
DRDY = "clocking" (high = 20us, low = 30ms)
Register settings:
REG0 = 0x0C = fosc/128 + Int Vref enable + Int Vref = 2.5V + Buffer disable + MSb transmitted first
REG 9 = 0x47 = Unipolar + Auto setting mode + Decimation default D10 to D8 = 7
Any suggestions?
Thank you
Fausto Bartra