This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/ADS1293: ADS1293

Part Number: ADS1293

Tool/software: TI C/C++ Compiler

Dear ti representative
I would to have the code for the EVM Ads1293 to use in a bluetooth device . currently the interface is with a USB type with the pc or lap top . we can easily modify it to sent our lab application.
Thank you

  • Hi Rashed,

    Thanks for your post!

    Unfortunately we do not have code available for communicating with a bluetooth device.

    Keep in mind that code is provided “as-is” and modifications/changes are not supported. Also note that this software is optimized for our evaluation platforms and therefore may not be well suited to end-equipment applications.