Part Number: ADS54J40EVM
Other Parts Discussed in Thread: DAC38RF82EVM
can ads54j40evm works with fpga virtex 6 ml605 ????!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADS54J40EVM
Other Parts Discussed in Thread: DAC38RF82EVM
can ads54j40evm works with fpga virtex 6 ml605 ????!!
Abdallah,
We have never tested a Virtex 6 ml605 with a JESD204B device EVM. I suggest you contact Xilinx to see if this platform has a JESD204B IP core. If I remember correctly, I thought the transceivers on this board do not support this standard but I am not 100% sure. If the board does support the standard, then you need to verify if the required signals used by the ADC are mapped to the FMC connector on the ml605.
Regards,
Jim
Jim,
I've been into confusion after your last reply, since from what i got here, and from Xilinx website, it shows me that ML605 support JESD204B :
www.xilinx.com/.../jesd2014-reference-designs.html and this as well.
I hope you can clarify it to me ASAP, and Thank you
regards,
Abdallah
Abdallah,
This is the latest from Xilinx:
"I believe way back in 2013 in the last days of our ISE software there was a version of JESD204B that worked on Virtex 6 devices (as found on the ML605).
This is no longer supported and Vivado has never supported Virtex 6 devices.
I will look to updating our webpages to remove mention of this".
Regards,
Jim