Part Number: DAC5682Z
Hi
I am currently working on a university project and want to use the DAC5682Z.
I have a question regarding the voltage level of the digital data input D[15..0]P/N.
The signal is generated from an FPGA as an LVDS 1.8 V signal. Can I connect that directly (with 100 ohm termination resistors) to the DAC, or do I need a level converter in between? and if so can you recommend one? I have researched as well as I could, but can't find any.
I have checked the data sheet 7.3 but don't quite understand it. Is the value a peak peak or an amplitude value?
Regards
Michelle