Part Number: ADC1173EVM
Got below question:
I'm using the EVB ADC1173EVM and I'm having important issue.
I'm supplying 5V, from power supply while supplying my own 3Mhz clock with output buffer disabled.
Power consumption is 5*20mA = 0.1W (without clock provided)
And 5*14mA = 70mW while supplying clock of 3Mhz.
- Why power consumption is higher without clock ? it should be other way around..
- According to Datasheet it should be 33mW @15Mhz. so I expected it to be around 10mW @3Mhz.