Part Number: DAC6574
Hello,
Our customer use the DAC6574.
They refer to the Absolute Maximum Ratings, have a question.
It is mentioned the Digital input voltage to GND up to VDD+0.3V.
Is this correct?
They use some devices with same I2C bus. They want to turn off the power individually.
If there is limit at Digital input, they can not use the DAC6574.
Best Regards,
Naoki Aoyama