We are using the IC in the VQFN package. Which capacitance is the minimum required at the REFP/REFM pins? According latest datasheet it shall be 10uF. However in the issue C of the datasheet (SLAS605) in Figure 70 there is a layout example with 1uF capacitance value. So, at least the drawing is not in-line with the text within datasheet. If I can safely change the capacitor value from 10uF to 1uF this would help much to accommodate with the layout guide line and to save PCB space (smaller package size). Thanks in advance! Regards Andreas