Part Number: ADC12DJ3200EVM
Other Parts Discussed in Thread: ADC12DJ3200
I am looking at some code that resembles JMODE0 Table 20. (page 66) of the ADC12DJ3200 documentation but I don't know where they get the bit ranges.
This is what is looks like:
s0 31:20 s8 19:8 s16 7:0 31:28 s24 27:16 s32 15:4 3:0
s2 63:52 s10 51:40 s18 39:32 63:60 s26 59:48 s34 47:36 35:32
s4 95:84 s12 83:72 s20 71:64 95:92 s28 91:80 s36 79:68 67:64
s6 127:116 s14 115:104 s22 103:96 127:124 s30 123:112 s38 111:100 99:96
s1 159:148 s9 147:136 s17 135:128 159:156 s25 155:144 s33 143:132 131:128
s3 191:180 s11 179:168 s19 167:160 191:188 s27 187:176 s35 175:164 163:160
s5 223:212 s13 211:200 s21 199:192 223:220 s29 219:208 s37 207:196 195:192
s7 255:244 s15 243:232 s23 231:224 255:252 s31 251:240 s39 239:228 227:224
Where do I find out the ranges? For example for s0 they have 31:20 where do they get this? Is this in the documentation?
Also is there a place I can get this so I can reverse engineer this pattern for JMODE 11?
Thanks,
Zach