Part Number: ADS7957
Hello,
my target is to set the ADS7957 IOs per SPI command. Problem: I can see the set output values neither on the SDO data (if this mode is selected), nor on the outputs.
I can confirm that the communication itself is working properly:
1)Power on Reset:
2)I set all GPIOs as output Frame: 0x400F
3) switch to Auto1 mode with Mux Channel output on SDO[15..12] Frame: 0x2800
==> I can see the channels being counted up (as expected)
Problem Case:
1)Power on Reset:
2)I set all GPIOs as output Frame: 0x400F
3) switch to Auto1 mode with GPIO Channel output on SDO[15..12] Frame: 0x281F (ALL GPIOS = 1) respectively Frame: 0x2810 (ALL GPIOS = 0)
4) sent permanently Auto1 steady mode Frame: 0x2000
==> There is no change in the signal level nor on the SDO data [15:12]
Could you please confirm that the initialisation messages are reasonable?
Is there any external circuitry that has to be foreseen for the GPIOs?
Thanks in advance for your time!