HI
when looking at the evaluation board user guide some of the items in the BOM table is listed as "NSC" does that mean that the components are not included on the board?
I have a problem with the 5223514-3 connector. No matter where I look the minimum amount of male connector, compatible with the one on the eval board, I can buy is 480 pcs. and I only need one. If the 5223514-3 connector is already mounted on the eval board is it possible to change it with some I can actally find a male connector for?
Alternatly can you recommend one that is compatable? I have looked at 223513-3, 223513-3 and 223514-3. I have even tried to order a sample from the manufactor by they are out of stock.
Regards Michelle