This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1274EVM-PDK: About operation on win10.

Guru 11255 points

Part Number: ADS1274EVM-PDK

Hi team.

We are looking for ways to work ''ADS1274EVM-PDK'' on win10.

When our environment is win10, is ''ADS1274EVM-PDK'' operable?

We are concerned about 2 point.

1. MMB0 motherboard works on win7 and XP only.

2. ADCPro™ works on winXP(and win7?).

There is no description of win10 for both.

If it could, please let me know.

If it couldn't,Could you tell me when will you update?

And then, If we use MMB3, Is it work on win10 ?

Sincerely.

Kengo.

  • Hello Kengo,

    ADS1274EVM only works with MMB0. The ADS127xEVM-PDK was originally released and tested with WIN XP and WIN7, but you should be able to get it to work on WIN10.  However, WIN10 by default enforces Driver Signature, which the ADS127xEVM-PDK will not meet.  WIN10 will prevent the USB driver installation which is needed for ADCPro to talk to the MMB0.

    If you cannot find an older machine running WIN7 or XP, then you should be able to temporarily disable Driver enforcement in WIN 10 by following this blog.

    I hope this is helpful.

    Regards,

    Keith N.

    Precision ADC Applications

  • Hi Keith.

    Thank you so much for your reply.

    I understood it and then I'll try your comment.

    Sincerely.
    Kengo.