This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1198: ADA1198 sampling rate variation and signal attenuation w.r.t. sampling rate

Part Number: ADS1198

Hi Brian

We are using TI's ADS1198 8 channels at 250SPS (4ms) rate with 5V AVDD and 4V as internal reference. ADS1198 is connected to a snapdragon via SPI and using android sensor framework to read the data on every DRDY signals. we are facing two issues in our system with ADS1198:

1. sampling rate (sampling period) varies drastically from 1ms to 6ms event though it is set at 250SPS (4ms)

2. signal attenuation happens on the actual signal and it varies as we change the sampling rate, with higher the rate lower attenuation

can you suggest the potential root causes that may lead to these issues and possible test scenarios to exactly pin-point source of the issue?

  • Hello Bhagvan,

    Thanks for your post and welcome to the forum!

    This is most likely caused by the digital filter being reset or a different SPI communication issue.
    Can you provide a scope shot showing /DRDY varying drastically?
    Is there any communication to the device near this event such as a reset?

    What is the frequency of your input signal?
    If you look at figure 21. of the datasheet you will see that there is a sinc filter will an attenuation rolloff dependent on fIN/fDR.
  • Hi Alexander

    Thank you very much for your reply.

    1. sampling rate variation looks like coming from varied handling of DRDY by the android sensor framework and we are now investigating it. we will come back if any further questions on this.

    2. our input signal is a real muscle EMG signals captured by the sensors attached to the arm skin, so it is 15 to 25Hz. so if the sinc filter has attenuation roll-off, how can we improve it? the datasheet shows that it can be changed by changing DR bits in config1 resister but DR bits actually changes the sampling rate which we want to keep at 250Hz fixed.

    thank you in advance for your effort.

  • Hi Bhagvan,

    Happy to help!

    Why do you want to keep the sampling rate fixed at 250Hz?
    Have you considered sampling at 500Hz and only reading every other sample?
  • Hi Alexander

    this idea looks interesting. let us try that out. however, we suspect that with 500Hz sampling rate, interrupt will be generated at every 2ms and even if we do reading at every alternate interrupt, our system still need to do some house keeping at every 2ms and which may break the timings of our sensor framework. but let's see the outcome.

    thank you again for your good suggestion.

  • You are welcome! Let me know how the testing goes!
  • Hi Alex

    we tried changing sampling frequency to 500Hz and then reading the samples at 250Hz. it definitely improves the frequency response. now the -3dB frequency shifts from originally 65Hz to 130Hz that's that good improvement. however, we have seen some strange issue with output signal quality. i input the pure sinusoidal wave and varied the frequency from 1Hz to 500Hz. at input frequencies which are integral divisor of 500Hz, e.g. 250Hz, 125Hz, etc the shape of the signal really goes bad, looks like it brings aliasing effect or introduces some harmonics of the input or sampling frequency to the oroginal signal. any solution?

  • Hi Bhagvan,

    Can you post a picture showing the output data waveform?
    Are you using the internal clock? If not, what is the frequency of your clock?
    The sinc filter has notches (or zeroes) that occur at the output data rate and multiples thereof. At these frequencies, the filter has infinite attenuation. I'm looking at figure 21./23./24. - but there are no notches lower than the datarate.

    There could be an issue with your input configuration, how you're reading/converting the data, or the device datarate is set incorrectly.

    Can you read a 10Hz sine wave input reliably?
  • Hi Alex

    Thank you for your reply.

    Attached are the data files 125Hz.xlsx250Hz.xlsxf digital output signals for 125Hz and 250Hz input sinusoidal signals. Yes, we are using the internal clock of the ADS1198. No external clock.

    we are reading the data via SPI on every alternate DRDY, with actual sampling rate of 500Hz and data reading output at 250Hz. after directly reading the data, we convert using floating point and transfer to a file. we do not see a problem at 10Hz signal. 10Hz data file: 10Hz.xlsx

    also we do not see a problem if used 250Hz ADC sampling rate and data read also 250Hz.

  • Hi Bhagvan,

    Happy to help!

    Looking at the graphs, I believe top left is input signal, bottom left is zoomed out output, top right is zoomed in output?

    This looks like data corruption - either the SCLK reads are overlapping DRDY pulses leading to truncation or an aliasing effect.

    Are you reading off of the DRDY pulses or timing? Was the varied handling of DRDY by the android sensor framework issue resolved/confirmed?

    Looking at the 250Hz graph, I see a few periods (~1329 to 2159) that look fine, then corruption (2325 to 2491), then fine, then corruption etc which makes me think there may be a timing issue.

    Do you see the issue for a 62.5Hz signal? 31.25Hz? What will the frequency of your signal be for production measurements?

    If you increase the output datarate to 1ksps and take every fourth sample, does the issue persist? If not then it may be a Nyquist issue. I'm not entirely sure how the math works out for sampling at half the output datarate like this. For reference, here's an article on Nyquist and Aliasing: e2e.ti.com/.../aliasing-in-adcs-not-all-signals-are-what-they-appear-to-be
  • Hi Alex

    in a particular file, all data is only for output. input for that output is always fixed at 2Vpp+1.5Vdc sinusoidal signal with frequency equal to that file name. in each file, the output data-set is captured for ~10 seconds recording and different graphs in the same file are nothing but a plot of different time length data-set from the same file starting from the first reading.

    SCLK reads are not overlapping with DRDY in any of the data-sets as we have had conformed that through logic-analzer on the SPI bus. that is also confirmed by not having the similar issue if we have input frequency e.g. 1Hz, 5Hz, 10Hz, 25Hz, etc...but only seen on 125Hz and 250Hz only. by the way we are reading off the DRDY pulses, not timing. we don't see the varied handling of the DRDY by android sensor framework anymore and that is confirmed that it is resolved.

    250Hz graph at left bottom is actually a onsecond data plotted and it actually does not represent 250Hz at all. all the data is completely messed up by the filter of the ADC. we do not see the proble at 62.5Hz and 31.25Hz. our frequency of interest is ranging from 10Hz to 200Hz.

    I too suspect some kind of aliasing effect by the ADC and sinc filter.

  • Hi Bhagvan,

    I see, thank you for the clarification.

    Great to hear that the sensor framework issue is solved and that you're reading off of DRDY.

    If you're max frequency of interest is 200Hz then sampling at least 2x the input frequency is a must. 500SPS (2.5x) should be sufficient, but some customers use up to 5x or 10x. However, like I said in my previous post - I am not positive how this works with discarding every other sample. Is it possible for your to read every sample to rule this out as the issue?

    What are the values of your RC anti-aliasing filter on the input?

    Can you share a schematic and register settings? I can contact you offline if you're not comfortable sharing on the forum.
  • Hi Alex

    we are not using any RC anti-aliasing filter as we think that sinc filter should work as anti-aliasing filter as it was explained in the datasheet. do you think we need the RC filter at every input?

    to send the register settings, let's sync-up offline.
  • Sent you an email.