Part Number: ADS54J42
Dears.
I am doing the temperature test of ADS54J42.
When the temperature is low and high, system ON / OFF test.
There are two problems.
What is the solution?
1) Room chamber
When it is low temperature(Less than -10 degrees), JESD204B LINK is connected to normal but data is not output.
When the temperature rises(above 5 degrees), it works normally.
2)Sync is not connected at high temperature(above 40 degrees).
The ADS54J42 configuration is shown below.
LMFS : 2242
SYSREF : 5.76Mhz
K : 16
LINE RATE : 3.6864Gbps
lane per link : 2
decimation : x2
BW : 75Mhz
Device Clock : 368.64Mhz
* Register Value
0x0000 0x81
0x0011 0x80
0x0059 0x20 # always write 1 to bit 5
0x4003 0x00
0x4004 0x68
0x60f7 0x01 # digital reset : self clearing reset
0x6044 0x00 # digital gain = 6dB
0x6041 0x16 # dec filter mode (bit 5, 2-0), DECFIL EN (bit 4)
0x604d 0x08 # DEC MOD EN (bit 3)
0x6052 0x80 # bus reorder en1 (bit 7)
0x6072 0x08 # bus reorder en2 (bit 3)
0x6000 0x01 # reset digital. Must issue after writes to 6800h
0x6000 0x00 # clear reset
0x4003 0x00
0x4004 0x69
0x6001 0x32 # SYNC(7), SYNC Register Enable(6), JESD Filter (bit 5-3), JESD Mode (bits 2-0) :"00110010"
0x6000 0x80 # set CTRL K
0x6006 0x0f # set K to 16 (write K-1)
0x6031 0x0a # output lane reorder to get data on DA0 and DA1
0x6032 0x0a # output lane reorder to get data on DA0 and DA1
0x6005 0x00 #
0x4003 0x00
0x4004 0x6a
0x6016 0x02 # JESD PLL Mode