I have an battery powered application that requires very low standby currents. Only one differential channel is required to the input mux will not be switched. My plan is to power up the system, run a calibration cycle on the ADC and put the device in standby. I would like bring the device out of standby, take a sample, go back to standby.
PGA = 16, 4.9152Mhz Xtal for ADC clock, single channel.
The real reason for the questions is to properly calculate the amount of power required by the system with a 5Hz sample rate. So if there is an easy way to calculate the power, that would be valuable information.
Now, the questions -
How much time is required to come out of standby, sample the analog signal, go back to standby ?
Is a settling time or recovery time required or suggested when coming out of standby ?
Is there a suggested software flowchart describing the steps (commands) required to do this most effectively ?
Will the ADC have max ENOB after one sample cycle or are multiple cycles required for maximum performance ?