Part Number: ADS1220
Other Parts Discussed in Thread: ADS1246, , ADS124S06, SN74LVC1G02, SN74LVC1G125
I have build a test board with two ADS1246 to sample two bridge sensors (in a ratiometric way) simoultaneously at a sampling rate of about 1kHz. The start of conversion is controlled using the START pin which are both connected to a PWM with 1kHZ frequency.
I would use the ADS1220 but it has no START pin. Can I send the START/SYNC (0000 100x) command helding both CS pin low at the same time?