hi,
i need help for initial configuration of register about DAC3482.
the dataclk is 245.52MHz,and the dacclk is 491.04MHz.
the paramter in my code is following :
addr_00 = 16'h0118,
addr_01 = 16'h010E,
addr_02 = 16'hF0C2,
addr_03 = 16'hA000,
addr_04 = 16'h0000,
addr_05 = 16'h0000,
addr_06 = 16'h3300,
addr_07 = 16'hF9FF,
addr_08 = 16'h0000,
addr_09 = 16'h8000,
addr_0A = 16'h0000,
addr_0B = 16'h0000,
addr_0C = 16'h0400,
addr_0D = 16'h4400,
addr_0E = 16'h0400,
addr_0F = 16'h0400,
addr_10 = 16'h0000,
addr_11 = 16'h0000,
addr_12 = 16'h0000,
addr_13 = 16'h0000,
addr_14 = 16'h0000,
addr_15 = 16'h1000,
addr_16 = 16'h0000,
addr_17 = 16'h4000,
addr_18 = 16'h280F,
addr_19 = 16'h0840,
addr_1A = 16'h0060,
addr_1B = 16'h0800,
addr_1C = 16'h0000,
addr_1D = 16'h0000,
addr_1E = 16'h1111,
addr_1F = 16'h1102,
addr_20 = 16'h2200,
addr_22 = 16'h1B1B,
addr_23 = 16'h07FF,
addr_24 = 16'h0000,
addr_25 = 16'h7A78,
addr_26 = 16'hB6B6,
addr_27 = 16'hEAEA,
addr_28 = 16'h4545,
addr_29 = 16'h1A1A,
addr_2A = 16'h1616,
addr_2B = 16'hAAAA,
addr_2C = 16'hC6C6,
addr_2D = 16'h0004,
addr_2E = 16'h0000,
addr_2F = 16'h0000,
addr_30 = 16'h0000;
Is there any errors?how to modify that?
And do you have some examples or projects with FPGA and DAC3482 about timming operation.
thanks a lot.