I am trying to connect the ZCU102 Ultrascale+ FPGA and the ADC12DJ3200EVM together so I can feed through test waveforms. Is there any documentation that talks about how to connect the FPGA and ADC EVM correctly?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am trying to connect the ZCU102 Ultrascale+ FPGA and the ADC12DJ3200EVM together so I can feed through test waveforms. Is there any documentation that talks about how to connect the FPGA and ADC EVM correctly?
Can anyone help me here? I am trying to connect the ZCU102 Ultrascale+ FPGA and the ADC12DJ3200EVM together so I can feed through test waveforms. Is there any documentation that talks about how to connect the FPGA and ADC EVM correctly?
Hi Zachary
We don't have information directly applicable to that EVM combination.
We do have a reference design for the ADC12DJ3200EVM with the KCU105 platform. That information is available in the Software section of the ADC12DJ3200EVM folder here:

I hope this is helpful.
Best regards,
Jim B
Thank you. However, my question is more about connecting the ADC to FPGA in a way that I can program both of them together. Currently, the ADC causes my FPGA to become unprogrammable. Is there some pin adjustments that need to be made to the ADC so that it can attach to the KCU FPGA? This would be helpful to reference for my design.
Thanks Jim. I put a jumper on the J27 (Jtag loopback) on the EVM and now the ADC and FPGA can both be programmed. If you could help me understand why this is the case that would be great.