Hello,
Let me confirm about how we should consider total error of gain.
* According to datasheet, there is following description.
1. gain error : +/- 0.2% of FSR (max)
2. gain temperture coefficient : +/- 1 ppm of FSR/degree
And also, I believe that accuracy of internal reference (25 ppm/degree at Type B) will be related to "gain error".
The question is,
Q1. When we concider total error of gain, should we concider only above three elements ?
Q2. If answer of above is yes, could you please tell us how we calculate total gain of error by using above elements ?
Thanks in advance,