Hello.
In one of my projects, I use the ADC12D1800 in NON-DES mode (using two independent data streams (I&Q)) with sampling clock of 1600Mhz and it works fine.
In other project (on the same (exactly the same) platform, again with two independent data streams), the clock is set to 1800Mhz, while the interface and the power-up sequence stay the same.
Although in TPM mode I get the correct patterns (i.e. my LVDS receiver is properly configured), the input data is corrupted.
I am aware of the special configuration registers when clock is above 1600Mhz, and also tried to re-configure and re-calibrate after power-up with no success.
I came to believe that maybe the initial power-up sequence somehow causes an in-repairable error which only hard reset may solve (and may not - the error is very frequent).
I will appreciate if you could issue a recommendation for a proper NON-DES 1800Mhz sampling clock scheme.
Thank you very much,
Itay.