Hi,
In order to suppress spurs at certain frequencies, we use the offset corrector like the following way:
1) Make sure no signal on inputs.
2) Enable offset corrector and wait for sometime to collect enough data for estimation
3) Freeze corrector
4) Now ADC can receive signal without spurs.
Instead of doing this procedure every time, we would like to make the calibration at factory and store the coefficients. In that case, we will be able to calibrate the ADC by only loading related coefficients without any extra calibration step (with no signal on input). Otherwise, while using the ADC in the field, at least for every startup, we need to apply a calibration procedure with no signal.
Is it possible to load/store offset coefficients?
Thanks,
Ozer